HVAC

Schneider Electric works hand-in-hand with our partners to develop dedicated HVAC solutions to meet the real-world needs of customers.

This site, dedicated to Schneider Electric’s HVAC OEM program is designed to help you understand and take advantage of the resources and expertise that is available. For HVAC OEMs this means having access to the valuable resources you need to be more competitive, when you need them most. Please use the links to the right to find out more. For more information, please contact your Schneider Electric sales representative or contact the HVAC program team online.

Features

Improve your HVAC system and save money with PID control

Uncontrollable changes both inside and outside of a building can impact efforts to maintain a desired temperature. Changes in occupancy, lighting, computer-equipment and outdoor temperature cause the set temperature in a building to fluctuate constantly. Incorporating PID control with variable-speed drives results in HVAC systems that are more efficient and save money.

Proportional control provides the output capacity of HVAC equipment matching the load requirements of a building. Savings can be realized in three major areas:

Maintenance

Reducing dependence on throttling valves and dampers for the mechanical adjustment of airflow output saves on the maintenance of temperature-control equipment.

Energy

Open-loop control equipment cycles on and off constantly, causing a peak in-rush current during startup. Closed-loop controls used in PID save energy by providing continuous operation of AC motors at lower speeds.

Money

Reducing pump and fan-motor speed reduces electricity costs.


For more information on PID control, email us at HVAC@us.Schneider-Electric.com.