Low Voltage Motor Control Center Direct Replacement Units
Upgrade your motor control centers with industry leading components, without replacing the structure and bus
Motor control center structures and internal bus work typically have a long life. Their unit racking systems are simple and most likely, in good shape. So why replace the entire MCC when problems arise?
New direct replacement motor control center units are available for many common vintage and current style MCCs. This approach minimizes outage time and reduces costs associated with having to match existing footprints for the removal and reinstallation of cables. You can also replace units one at a time over an extended period, which provides an overall equipment upgrade on a limited maintenance budget.
Following is a partial list of OEM models in which direct replacement units are available:
|
-Allen-Bradley: Centerline® 2100 (pictured) |
-General Electric: 7700 and 8000 Series |
|
-ITE – Gould – Telemecanique: Series 5600* |
-Square D Model 4 |
|
-ITE – Imperial – Telemecanique: Series 9600 |
-Westinghouse and Cutler-Hammer: Type W |
|
*Design acquired by Schneider Electric in 1988. |
|
Features of an MCC Direct Replacement Unit
-
New “bucket” and plug-on stabs designed by Square D Services
-
Furnished with a Square D circuit breaker or fusible disconnect switch, as specified
-
Includes the industry leading Type S Square D starter and Square D control circuit components
-
New door with rotary disconnect handle
-
Some styles will have a linear handle, such as the Square D Model 4
-
-
Interlock to prevent bucket from being removed while disconnect is closed
-
Drawings provided per Schneider Electric standards
-
Designed and tested per UL 845, Underwriters Laboratories Standard for Motor Control Centers
-
Options for an MCC direct replacement unit include solid-state overload, circuit breaker or fusible disconnect, and door-mounted pilot devices.
Retrofit Units. When a direct replacement unit is not available, we can retrofit a genuine OEM bucket with all new Square D components. The genuine OEM stab assembly is reconditioned to like-new condition and the bucket is painted white enamel. All work is performed by factory-trained Square D Services personnel.