Walk-In Enclosures (Power-Zone Center)

Custom designed enclosure designed for the protection of equipment in an outdoor or adverse environment.

The Walk-in Enclosure (Power-Zone® Center) is a custom designed Enclosure designed for the protection of equipment in an outdoor or adverse environment.

  • The custom design of the Square D® enclosure allows virtually any size layout or configuration.
  • They are typically built and shipped in one module requiring no assembly at the job site.
  • All equipment installed and wired as required.
  • The inside of the enclosure can be environmentally controlled.
  • Square D warranty coverage for the entire enclosure and equipment.

For more information on specific enclosures, use the links on the left to select an enclosure type.

Square D logo

For a complete listing of documentation for this product, please consult the Technical Library.

Brochures
Power Zone Center House 6052BR9401R6/06
Instruction Bulletins
NEMA 3R Walk-in Low Voltage Switchboard/Switchgear Installation 80298-156-01