SEPAM Relay Training
Industrial Medium Voltage Relay Training
Square D SEPAM™ Industrial Medium Voltage Relay Training
Overview (4 Days) Class Number: 3000PLU1SEP
An introduction to SEPAM MV protective relays with emphasis on installation, operator interface, use of SFT2841 commissioning software, communications, basic protection, start-up, troubleshooting and maintenance.
Course content:
- Defining protective relaying and its uses
- Introduction and features of the SEPAM hardware with emphasis on understanding the application choices, relay selection and ANSI protective functions
- SFT2841 commissioning software including programming relays off-line, on-line and across a network. Use of relay configuration files.
- Presenting and analyzing values, alarms events and waveform captures
- Basic description of optional pre-configured control schemes e.g. bus transfer, ZSI, ATS, control matirx, logic equation editor, and logic interface
- Start-up, troubleshooting and maintenance
How to register:
- Visit www.powerlogic.com/training to link to the Power Management University website.
- Or call us at 615-287-3304 and we will be happy to register you for a course over the phone. FAX: 615-287-3403