Modicon Quantum Ethernet I/O System
Introduction to Quantum Ethernet IO System
PlantStruxure™ is a Schneider Electric program specifically designed to address the key challenges of many different types of users — including plant managers, operations managers, engineers, maintenance teams, and operators — by delivering a system that is scalable, flexible, integrated, and collaborative. Ethernet is the backbone around which the Modicon™ Quantum™ PLC offer connects a Modicon Quantum local rack to remote I/O drops. Use the links below to explore the benefits of incorporating this solution:
| > Flexible, cost effective | > Deterministic | > Open standard | > High reliability |
| > Higher density, smaller footprint |
> Cost effective | > High availability | > Simple upgrade |
This feature, known as Modicon Quantum Ethernet I/O or QEIO, is a set of new features and new product version. For more information, follow the links below:
Applications
- Mining and Mineral
- Material Handling
- Oil & Gas
- Chemical
- Petrochemical
- Transportation
- Water Wastewater
- Food & Beverage
- Metals
- Infrastructure