Modicon Momentum PLC and Distributed I/O

ProWorx 32 or Concept PLC programming software
Ideal for PC-based control, distributed control, distributed I/O and traditional standalone PLC control

The small footprint and open architecture of the Modicon™ Momentum™ PLC product line make it extremely versatile for a variety of automation applications. Modicon Momentum PLC options and accessories include: I/O bases, processor adapters, option adapters and communication adapters that are interchangeable and snap together to deliver optimal flexibility throughout the control system lifecycle.

As a distributed control solution, the M1E module delivers the performance of a full function, real-time controller for standalone and distributed system configurations in one money-saving unit. This is especially useful where high-speed distributed control is required. The Modicon Momentum PLC offers selected I/O bases, processors and communication modules with conformal coating - ideal for applications with harsh or humid environments that require a small footprint.

Using Ethernet as its communications backbone, the Modicon Momentum M1E Processor delivers all the performance benefits of real-time control. Its open architecture makes it the first truly universal controller for distributed I/0, compatible with many of the major fieldbus and control network environments. With the release of the Modicon Momentum M1E Connexium™ module (171CBB97030), this interoperability is extended even farther. An integral Ethernet port in the M1E allows users to perform a wide range of functions over Ethernet, including data acquisition, peer-to-peer communications and I/O scanning. Five embedded webpages enable the use of a standard web browser to read status and diagnostic information from the processor. Learn more about the Modicon Momentum M1E Connexium Module.

Key documentation

Applications

  • Simple Machine Control
  • Material Handling
  • Oil & Gas
  • RTU
  • Building Automation

For a complete listing of documentation for this product, please consult the Technical Library.

Brochures
Momentum: the flexibility to adapt with your business AUTB10216124EN
Schneider Electric system monitors and controls gas well production pressure 8000AC0517
The Industrial Facility Evaluation Program 8000BR1110
Catalogs
Modicon Momentum automation platform - Catalog 2011 MKTED205061EN-US
drawings
PLC Controllers -Momentum wiring for the 170aai14000 and 170aai52040 io base
PLC Controllers-Momentum wiring for the 170adi34000 and 170adi350000 io base
PLC Controllers-Momentum wiring for the 170adi54050 and 170adm350xx io base
PLC Controllers-Momentum wiring for the 170adm39030 and 170ado54050 io base
PLC Controllers-Momentum wiring_for_the_170adm69050_and_170ado34000_io_base
PLC Controllers-Momentum wiring for the 170ado35000 and 170ado53050 io base
PLC Controllers-Momentum wiring for the 170ado73050 and 170amm09000 io base
PLC Controllers-Momentum wiring for the 170ado74050 io base
PLC Controllers-Momentum wiring for the 170aao12000 and 170aao92100 io base
PLC Controllers-Momentum wiring for the 170adi34000 and 170adi350000 io base
PLC Controllers-Momentum wiring for the 170adi54050 and 170adm350xx io base
PLC Controllers-Momentum wiring for the 170adm37010 and 170adm39010 io base
PLC Controllers-Momentum wiring for the 170adm39030 and 170ado54050 io base
PLC Controllers-Momentum wiring_for_the_170adm69050_and_170ado34000_io_base
PLC Controllers-Momentum wiring for the 170ado35000 and 170ado53050 io base
PLC Controllers-Momentum wiring for the 170ado73050 and 170amm09000 io base
PLC Controllers-Momentum wiring for the 170ado74050 io base
PLC Controllers-Momentum wiring for the 170aao12000 and 170aao92100 io base
PLC Controllers-Momentum wiring for the 170adi34000 and 170adi350000 io base
PLC Controllers-Momentum wiring for the 170adi54050 and 170adm350xx io base
PLC Controllers-Momentum wiring for the 170adm37010 and 170adm39010 io base
PLC Controllers-Momentum wiring for the 170adm39030 and 170ado54050 io base
PLC Controllers-Momentum wiring_for_the_170adm69050_and_170ado34000_io_base
PLC Controllers-Momentum wiring for the 170ado35000 and 170ado53050 io base
PLC Controllers-Momentum wiring for the 170ado74050 io base
PLC Controllers-Momentum wiring for the 170aao12000 and 170aao92100 io base
PLC Controllers-Momentum wiring for the 170adi34000 and 170adi350000 io base
PLC Controllers-Momentum wiring for the 170adi54050 and 170adm350xx io base
PLC Controllers-Momentum wiring for the 170adm37010 and 170adm39010 io base
PLC Controllers-Momentum wiring for the 170adm39030 and 170ado54050 io base
PLC Controllers-Momentum wiring_for_the_170adm69050_and_170ado34000_io_base
PLC Controllers-Momentum wiring for the 170ado35000 and 170ado53050 io base
PLC Controllers-Momentum wiring for the 170ado73050 and 170amm09000 io base
PLC Controllers-Momentum wiring for the 170ado74050 io base
PLC Momentum Controllers Fig-100
PLC Momentum Controllers Fig-101
PLC Momentum Controllers Fig-102
PLC Momentum Controllers Fig-99
PLC Momentum Controllers Fig-100
PLC Momentum Controllers Fig-101
PLC Momentum Controllers Fig-102
PLC Momentum Controllers Fig-99
PLC Momentum Controllers Fig-100
PLC Momentum Controllers Fig-101
PLC Momentum Controllers Fig-99
PLC Momentum Controllers Fig-100
PLC Momentum Controllers Fig-101
PLC Momentum Controllers Fig-102
PLC Momentum Controllers Fig-99
urls
The links below are to the Schneider Electric global document repository. Note that some of the products and information available at this website may not apply in North America
Momentum Controllers Brochures
Momentum Controllers Catalog Pages
Momentum Controllers Catalogs
Momentum Controllers Certificates
Momentum Controllers Resolutions
Momentum Controllers Tech Pub