Underground Service Wireways For MP Meter-Pak Meter Centers

Convenient solution for protecting a utility's underground service conductors that terminate in MP Meter-Pak meter centers.

Underground Service Wireways are a convenient solution for protecting a utility's underground service conductors that terminate in MP Meter-Pak™ meter centers. These non- load bearing Underground Service Wireways are intended for use only as a means to cover and secure service entrance cables prior to entering a wall-mounted Meter-Pak device. The units connect easily to any MP Meter-Pak meter center by attaching a tapped hub provision in the bottom endwall of the metering device.

Features
  • Cover latch accommodates up to three different types of utility seals. All locking provisions are made of durable, corrosion-resistant stainless steel to meet strict, utility security requirements.
  • Easily mountable to MP Meter-Pak meter center's underground, bolt-on hub provisions using supplied hardware. Open bottom with ½" rolled edge reduces possibility of cutting conductor insulation. In addition, wireway covers are secured by latching means - no screws to lose.
  • Gasketed, bushed openings in top provide watertight seal between the wireway and MP Meter-Pak meter center. Wireways are constructed of 14-gauge, painted galvanneal steel for superior corrosion protection in all applications.
Square D logo