Power-Ground and Ground Modules

Where room ground extensions and power receptacles are both required.

Where room ground extensions and power receptacles are both required, these modules offer convenience and saves much labor in field wiring. The unit includes four power receptacles, four twist-to-lock ground jacks, and a ground bus with a generous number of lugs for external ground connections.

Power/Ground Modules (To Fit Gang Boxes)

The modules can be used where additional ground jack receptacles and powe lock receptacles are needed, but where lugs for hard grounding of non-electrical items are not required.

Master Grounding Station Module

This unit can be used as a collection point for grounds in a large area such as a coronary care or intensive care ward. Primary application is where the equipment ground bus in the emergency distribution panel is not conveniently located or cannot accept the large number of connections, which may be required for the area.

Ground Modules

Ideal for room ground bus extensions to make ground connections in large operating rooms convenient. These units contain four ground jack receptacles and ground bus.

Square D logo