Digital Clocks and Timers

Uniquely adaptable to the hospital environment.

MCT Series timepieces are designed for areas requiring rapid and precise time measurements. They are compact, solid-state, and easily readable from 30 feet away. The MCT series of clocks/timers is designed for component mounting in various pieces of equipment such as modular walls, consoles, surgical facility panels, or building walls. This series is packaged in a durable flush mounting phenolic case.

Dual Display Clock/Timer (MCT-12B) and Control Panel (MCT-CT)

This dual timepiece is designed for surgical or patient care areas where simultaneous clock/timer displays are needed. The upper display is a time clock and the lower display is an elapsed timer. Controls for both displays are on the face of the unit. The display can also be remotely controlled by the MCT-CT remote control panel.

Surgical Chronometer (MCT-14B) and Control Panel (MCT-4RC)

Chronometer includes elapsed time indicators for the operating room. This unit has three elapsed-time indicators and one clock integrated into a single, compact enclosure. The MCT-RC remote control panel can be mounted in a location selected for accessibility.

Square D logo

For a complete listing of documentation for this product, please consult the Technical Library.

Instruction Bulletins
Iso-Gard™ IGT Dual Clock/Timer and IGT1550 Remote Control MED90110102