ASi Interface

Asi Interface
AS-Interface Safety at Work

Capable of managing safety functions up to category 4 of standard EN-954-1/ISO 13849-1 and conforming to SIL 3 of standard IEC 61508, the AS-Interface “Safety at work” system meets the needs of the most common safety monitoring applications.

Read More