Intelligent Load Centers

Kohler Power Systems Group has partnered with Schneider Electric to develop a superior solution to managing electrical loads to enhance the performance of a back-up power system.

Electrical Protection for Back-Up Power

Protecting your home from power outages is essential to maintaining home functions, such as lighting and HVAC systems. Kohler Power Systems Group has partnered with Schneider Electric --makers of Square D brand electrical products-- to develop a superior solution to managing electrical loads to enhance the performance of a back-up power system.

The Square D Intelligent Load Center senses when utility power is interrupted. Coupled with a quality stand-by power source such as a Kohler generator, the Intelligent Load Center automatically switches to back up power with automatic transfer of power from the utility company to the generator. You choose the essential circuits requiring power during an outage and the Intelligent Load Center assures back up power for those circuits.

The Square D Intelligent Load Center protects your home, while Kohler generators provide the cleanest power quality available in automatic standby generators for added preservation of sensitive electronics. This system assures that power interruptions won’t interrupt your quality of life.

In addition to the standard features you expect from Square D QO Load Centers, the Square D Intelligent Load Center features automatic switching between main and alternate power source (such as a backup generator).

For more information on Square D Intelligent Load Centers, please contact your local Square D sales representative.
 

Square D logo