Backed-Out Neutral Screws For QO and HOM Load Centers
A new feature on QO® and Homeline® load centers will now save labor and installation time for customers. When installing Square D load centers they will no longer have to loosen all the screws on the neutral bars as previous installations have required. QO and Homeline load center’s neutral bars will now provide backed-out neutral wire binding screws which meet all applicable UL and NEC requirements. This backed-out screw position is available now on the ground bar kits and will soon be available on the load centers and ground bars installed in the load centers.
Identification
To identify this new feature look for the "STARBURST" on the carton label.

Implementation Timeline
The load center neutrals and installed ground bars will come with backed-out neutral wire binding screws in stages in order to work through existing inventory. (PK Ground bar kits currently come with the wire binding screws backed-out.) There will be six stages of release for the load centers and factory installed ground bars.
Release Stages |
Load Center Type |
Estimated Release Date |
| 1 | PK-Ground bar kits | Currently Available |
| 2 | Homeline High Amp (150-225A) | December 2008 |
| 3 | Homeline Low Amp (125A & down) | January 2009 |
| 4 | QO High Amp (150-225A) | February 2009 |
| 5 | QO Low Amp (125A & down) | March 2009 |
| 6 | QO Three - Phase | March 2009 |