ServicePak Power Outlets
Provides temporary power connection at construction sites and recreational vehicle parks.
Used to provide temporary power connection at construction sites and recreational vehicle parks. Each receptacle is protected by either GFCI or standard QO® circuit breaker in compliance with NEC requirements. These panels include the following features:
- Rainproof enclosure
- 10,000 RMS symmetrical ampere short circuit current rating
- UL Listed as suitable for use as temporary site service equipment
- Neutral bonding provisions included
- Enclosures with provision for field installable type "B" hubs
For a complete listing of documentation for this product, please consult the Technical Library.