Thermostats

C-Bus™ Programmable 4 Zone Thermostat
C-Bus™ Programmable 4 Zone Thermostat

C-Bus™ Programmable 4 Zone Thermostats are used to regulate the air temperature of up to four separate zones (plus an unswitched zone) by controlling heating/ventilation/air conditioning (HVAC) equipment. The unit can schedule up to four set points during a day, and unique schedules can be programmed for each day of the week. The unit monitors the air temperature using its internal temperature sensor or optionally via an external C-Bus temperature sensor.

Read More
C-Bus™ Basic Single Zone Thermostat
C-Bus™ Basic Single Zone Thermostat

The C-Bus™ Basic Single Zone Thermostat regulates the air temperature of a particular environment. The unit may be controlled via other C-Bus devices such as wall switches or a touch screen, or it may operate independently. The air temperature is monitored by the unit's temperature sensor or optionally via an external C-Bus temperature sensor.

Read More