Audio Distribution Unit

The Audio Distribution Unit is an optional device that can be used in conjunction with the C-Bus Multi Room Audio System to further enhance the C-Bus enabled audio product family.

Related Documents & Downloads

Features

  • Distributes a single stereo audio source to C-Bus Audio Amplifiers via a digitized signal over Cat-& cable
  • Does not require any C-Bus programming (hardware only)
  • One stereo analog audio source input (2 X RCA)
  • One digital audio output (for up to eight zones) (RJ45)
  • Output can be looped between C-Bus Audio Amplifiers
  • IR emitter port for transmitting remote signals