C-Bus Software Downloads

We are happy to offer our most common software downloads below. You can locate your desired software in the fully expanded 'tree' format below, or you can click a quick link in the navigation column to the left to narrow the list to your desired product or category.
Further information on any C-Bus download can be found by contacting
Tech Support.

C-Bus Ripple software is an application you run on your personal computer to stream music to an MRA Matrix Switcher. The software will catalogue your music collection and allow you to sort it in many ways including album art. This also allows advanced control of music selection via C-Bus.

C-Bus Calculator enables the designer of any C Bus Network to confirm that the critical network operating parameters are within
acceptable limits.  

C-Bus Calculator Set up enables the designer of any C Bus Network to confirm that the critical network operating parameters are within acceptable limits.  

C-Bus Diagnostic Utility can be used for diagnosing problems with C Bus installations.  

C-Bus Drawing Templates are in the following formats: AutoCad Templates (DWG) and Visio Stencils (VSS)  

C-Bus Infrared Commissioning Software (CIRCA) is used to commission C Bus IR Devices. Software allows the user to select IR codes
and assign them to particular output channels on an IR Device and make associations b/w IR codes and C Bus events.  

C-Bus IP Utility software is used for configuring IP based C Bus devices, such as the C Bus Network Interface (CNI).  

C-Bus Toolkit software is an application you run on your personal computer to configure and commission C Bus Installations.

DLT Simulator is a stand alone tool that allows users to create customized bitmap pictures of 'real' DLT LCD screens, for inclusion in specifications or as built documents. Tool is unsupported and is not linked to Toolkit or Clipsal software.  

Home Gate software provides a powerful and simple to use interface to C Bus via a standard PC, with the ability to tailor the appearance and operation of the user interface to a residential client's requirements.  

IR Reader is used to learn IR commands from remote controls to use with the Marpa software.  

Lantronix Device Installer provides users a single applications with a graphical interface and utilizing Microsoft's .NET Framework to access various configuration functions for Lantronix networking products.  

The Multi Room Audio Rapid Programming Application (MARPA) is used to configure the Multi Room Audio Matrix Switcher.  

PICED software is used to configure the following products: Monochrome Touch Screen, Color Touch Screen, Pascal Automation Controller (PAC).  

Schedule Plus software provides a powerful and simple to use interface to C Bus via a standard PC, with the ability to tailor the appearance and operation of the user interface to a commercial or industrial client's requirements.  

The Telephone Interface Commissioning Application (TICA) is used to configure the C Bus Telephone Interface (CBTI).  

TICA Telephone Interface Users Guide