Laser Service Program
The Square D® brand represents a commitment to provide the best electrical products in the industry to our customers.
Combination starters can be configured in quick and easy steps:
Program Overview
When you choose to order combo starters on the 3-day or 5-day Laser™ program, Square D will drop ship the devices from the Monterrey, Mexico factory or the Mechanicsburg, PA warehouse for delivery on the third or fifth business day after receipt of the order by Square D. As an example of the 3-day program, if the order is received on Tuesday of week one, it will be on the job site Friday of the same week. For the 5-day program, if the order is received on Tuesday of week one, it will be on the job site Tuesday of the next week. Please note Laser™ excludes Alaska, Hawaii and Puerto Rico.
How do I order a 3-day or 5-day Laser™ combination motor starter?
The only option available for ordering is the newly revised NEMA FV Combination Starter selector. By selecting Laser™ (3-day or 5-day) from the delivery program question, all available options will be listed in subsequent questions. Please contact Schneider Electric Distributors to help you with ordering the products.
Will the catalog number change?
The product selector will place the Form letter “Z3” for three day or “Z5” for five day at the end of the catalog number on the order paperwork only. The device and carton label will not reflect the Form letter “Z3” or “Z5”.
Which combination motor starters qualify for 3-day and 5-day Laser™ program?
All 8538 (SBG,SCG,SDG,SBA,SCA and SDA) melting alloy on solid state overload relay non-fused and fused (H,K) disconnect switch style, NEMA sizes 0 – 2 in NEMA type 1 and 12/3R enclosures. Click here for the product selector
All 8539 (SBG,SCG,SDG,SBA,SCA and SDA) melting alloy on solid state overload relay circuit breaker style, NEMA sizes 0 – 2 in NEMA type 1 and 12/3R enclosures. Click here for the product selector
Are factory modifications available in the3-day or 5-day Laser™ program?
The most common factory modifications are available in this program. They are a follows:

What control power options are available?
V02S = 120V (separate source)
V03 = 240V (common source)
V06 = 480V (common source)
V08 = 208V (common source)
V80 = 240/120V (CPT)
V81 = 480/120V (CPT)
V84 = 208/120 (CPT)
Do I pay for premium shipping when I order via the Laser™ program?
The order point location will assemble the order so that there will be adequate time to get the product to the jobsite as scheduled using ground transportation. If for whatever reason standard routing will not get the combos to the jobsite by the third or fifth day after receipt of the order, Square D will pay for premium routing.